中文 | Deutsch | Español | Français | Italiano
Site Map | Contact Us | Index
Home  |  Products & Solutions  |  News Center  |  e-commerce  |  Support
Login | Register
[Advanced]
link to related website
Export information

Export information

(Previously embargo-exempt certificate)

Certificates for German exporters concerning SIMATIC products exempt from export authorization (in German only).
Detailed information (files in PDF format)

Additional information on SIMATIC PGs and Industrial PCs

The high speed of innovation in the memory and processor sector would necessitate a continuous demand for information about the list of goods. For this reason, the German Federal Authority for Trade and Export Control has deposited a "Recoding Directory for the Export List" at the customs offices, the current version of which contains a statement concerning PCs on page 168. This states that digital computers (a definition that covers PGs/PCs) are not to be included in the Export List and are therefore exempt from export authorization,

if they do not contain encryption, are not protected against compromising radiation, and do not exceed the following limit values:
1. at an "adjusted peak performance" (APP) of less than 0.75 weighted Teraflops (WT), (e.g. all Pentium types, 80486, all MPC types and 21164 types (Alpha chip series))"
2. with communication equipment not included in items 4A003g or 5A002 of the Export List

This and the next page of this recoding directory also stipulate that all printers, plotters, screens and monitors, digitizers, mice and trackballs, scanners and barcode readers as well as keyboards and light pens, disk memories and central storage (if a spare part of an embargo-exempt computer) are not to be included in the Export List. Since these directories are available at all Customs Offices, it is not necessary to present your own information on the list of goods in order to facilitate export.

SIMATIC Components
SIMATIC S7-200:
CPU 210/ 212/ 214/ 215/ 216, EM 231/ 232/ 235
PDFNr.08/00210
SIMATIC S7-300:
CPU 312IFM/ 313/ 314 314IFM/ 315/ 315-2DP/ 316/ 318
PDFNr.08/00211
SIMATIC S7-300:
SM 331/ 332/ 334, FM 350-1 / 350-2/ 351/ 352/ 353
PDFNr.08/00215
SIMATIC S7-300:
FM 354/ 357 / 357L
PDFNr.08/00216
SIMATIC S7-400:
CPU 412-1/ 413-1/ 413-2DP/ 414-1/ 414-2DP/ 416-1/ 416-2DP/ 417-4
PDFNr.08/00213
SIMATIC S7-400:
CPU 417H, SM 431/ 432, FM 450-1/ 451/ 452/ 453/ 455
PDFNr.08/00214
SIMATIC C7:
C7-621/ 621 ASi/ 623 623A/ 623P 633P/ 633DP/ 624 /624P
PDFNr.08/00209
SIMATIC C7:
C7-626/ 626A/ 626P/ 626DP/ 626PDP/ 634P/ 634DP
PDFNr.08/00212
  
Responsible:
A&D LEC ECC, Nuremberg-Moorenbrunn Mr. Morawietz, Tel. 0911-895-2546
Version 01/2008
Print
   

© Siemens AG 2001-2008 - Corporate Information - Privacy Policy - Terms of Use