Products & Technology - Industry Automation and Drive Technologies Overview - Siemens  |   12/02/2008 1:38 AM  
Hide Images  |  Print
New service package "Sinumerik Manufacturing Excellence"
"Excellence" Makes Its Debut
"Excellence" Makes Its DebutSiemens has developed a new service package for manufacturers and operators of machine tools - Sinumerik Manufacturing Excellence.

UGS PLM Software
Provider for the Complete Product Lifecycle
Provider for the Complete Product LifecycleSiemens is now the only supplier in the world to offer integrated systems and solutions for the entire product lifecycle over the complete value creation chain - from development, production and sales to service. This follows the acquisition of UGS Corp., Plano, Texas, USA, a worldwide leading provider of software and services for the digital factory, CAx technologies and digital product data management (PDM).

With Plant Intelligence to universal transparency and high productivity
Efficient Decisions
Efficient DecisionsProduction processes are becoming increasingly complex. Fast product changes, fluctuating plant workloads and growing quality demands are just some of the factors which can have a negative influence on the productivity of a plant. To largely avoid this, frequent decisions have to be made - on all levels of a company and in real time as far as possible.

Dematic develops an asset management solution with RFID
When Containers Send Radio Signals
When Containers Send Radio SignalsThe new EPCglobal radio frequency identification standard also gave impulses for the industrial RFID users. Low cost data media, long reading range and worldwide availability are convincing arguments for the technology. Dematic, a leading provider of RFID-controlled logistics systems, integrates the products into innovative solutions in a new technology center.

Accurate dimensioning of machines and systems with Safety Integrated
Economical Safety
Economical SafetyEnsuring safety in automatic processes is not only a question of human obligation but also of economic reason. According to this principle of Werner von Siemens, Siemens Safety Integrated offers comprehensive systems for the production and process industry which can be combined with optimum services for all phases of the life of a safety system or machine.

Certified safety components simplify press automation
Safe Pressing
Safe PressingThe high safety standards in presses demand the fastest response times from the controller and a defined sequence of safety functions. The press safety library makes automation of press safety functions even easier and more economical. The user also has a much lower engineering effort - from the concept phase to the utility model testing.

Trouble-free RFID operation by Simatic RF-Manager
Mediator Between the Levels
Mediator Between the LevelsThe main job of RFID systems is the automatic recording of goods and objects. However, the full potential of this new technology cannot be exploited until the read data are used and networked intelligently. To do this, RFID middleware such as the Simatic RF-Manager takes over the role of mediator between the writers/readers and master IT systems.

ALPHA 400-ZS and BETA Low-Voltage Protection Covers Every Project Requirement
Triple pre-meter protection
Triple pre-meter protectionBack in 2006 the TAB 2000 (Technische Anschlussbedingungen - Technical Connection Conditions) were modified to permit the use of fuses in the pre-meter area again. Now the release of the TAB 2007 is imminent, which makes the new lightweight and easy to install meter cabinets Alpha 400-ZS in conjunction with Beta low-voltage circuit-breakers an attractive option in more than one respect. After all, they enable the users to respond to customer requirements even more flexibly by providing them with three solutions for the protection at the intermediate meter: Selective main branch protective circuit breaker (SHU), MINIZED switch disconnector or NH00 fuses.

Safety Integrated fulfills latest safety standards
Trendsetter in Safety Matters
Trendsetter in Safety MattersApplications in the area of machine safety and process technology, as well as modern automation process technologies demand a high degree of safety for operators, machines and the environment. A sophisticated safety concept plays an important role particularly for the high feed speeds typical of today's woodworking industry. Users can therefore choose from numerous Safety Integrated functions.

Photovoltaic systems as alternative sources for electrical power
Harnessing the Sun's Power
Harnessing the Sun's PowerPhotovoltaic systems can be used in many different ways on buildings. Installed on the roof, on the facade or on the parking garage, they generate "green power", which is now in more demand than ever before.