Deutsch
Sitemap | Contact Us
Home  |  Products & Solutions  |  News Center  |  e-commerce  |  Support  |  About Us
Login | Register
[Advanced]
Publications
Press Center
Analyst Relations
Events & Trade Shows
Newsletter
Central Topics
PROFINET
Drive Technology
Automation Systems
Communication / Networks
Low-Voltage Controls and Distribution
Process Automation
Sensors
Power Supplies
Safety Integrated
Services

PROFINET

Company-wide automation and uniform communication with PROFINET, the open Industrial Ethernet Standard from PROFIBUS International.
SIMATIC ET 200M Available for PROFINET
IM 153-4 PN interface module
The IM 153-4 PN interface module now enables connection of the ET 200M distributed I/O system to PROFINET. In addition, the 153-4 module has an interface with integral 2-port switch and T functionality in the power supply. Up to 12 modules can be plugged in within one station, saving space in the control cabinet. The channel density can also be significantly increased by 64-channel modules (64 DI and 64 DO).
White Paper: PROFINET in the Process Industries
PROFIBUS & PROFINET International
Having proven its value in factory automation, industrial Ethernet is now emerging as a viable solution in the process industries as well. A new ARC White Paper entitled Arrow right"PROFINET in the Process Industries" appeared in April 2007.
SIMOTION V4.1 and PROFINET for High Performance in Machine Automation
SIMOTION V4.1 and PROFINET for high performance in machine automation
Version 4.1 of the SIMOTION Motion Control System features extended PROFINET functions for modular machine concepts, enabling electrical and hydraulic drives to be synchronized with each other. In addition, controllers can be configured simultaneously at the same PROFINET interface as IO Controller and IO Device. By means of controller-controller communication via PROFINET, SIMOTION V4.1 permits axis synchronization between several controllers.
PROFINET IO – Diagnosis of IO Devices
The spread of distributed automation systems with PROFINET has also seen a growth in the significance of the monitoring and diagnostics of such systems. STEP 7 offers a range of internal system functions in this regard for diagnosing PROFINET IO devices. One application example uses two different solution approaches to show how this task can be implemented within the STEP 7 user program and displayed on a SIMATIC HMI system.
SIMATIC ET 200S with Direct FO Connection
The new IM 151-3 PN FO interface module features integrated POF (poly- mer optic fibers) interfaces and utilizes the proven SC RJ cabling system which facilitates direct connection of the SIMATIC ET 200S product family to an optical PROFINET network. This means that for the first time both standard modules as well as fail-safe PROFIsafe modules can be operated on the ET 200S with a direct optical fiber connection. The integrated 2-port switch makes it easy to create linear topologies which are based on the machine or plant structure.
Page:   1  |  2
Print
   

© Siemens AG 2001-2008 - Corporate Information - Privacy Policy - Terms of Use